990-5940H-001

Connect the Power Cables in the 30-40 kVA 400 V / 15-20 kVA 208 V UPS

  1. Ensure that all breakers are in the OFF (open) position.
  2. Remove the lower plate.

    Rear View

  3. In dual mains systems, remove the three single mains brackets.
  4. Route the power cables through the bottom of the UPS.
  5. Connect the PE cable to the PE busbar.
  6. Connect the input cables, output cables, and bypass cables (if applicable).
  7. Connect the battery cables if the UPS should have external batteries for extended runtime.
    NOTE: Ensure that the type and number of blocks are the same as the internal batteries.
  8. Reinstall the lower plate.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.