990-5940H-001

Installation Checklist

  • The UPS and batteries are free of damage.

  • The UPS has been installed in a temperature controlled indoor environment free of conductive contaminants.

  • The UPS has been installed on a non-flammable, level and solid surface that can support the weight of the cabinet.

  • Upstream protection is installed according to Required Upstream Protection and Cable Sizes – 3:3 UPSs or Required Upstream Protection and Cable Sizes – 3:3 UPSs and local regulations.

  • Power cables have been connected according to the procedures in this manual.

  • Signal cables have been connected according to the procedures in this manual.

  • Battery cables have been connected according to the procedures in this manual.

  • All protection covers have been installed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.