990-5940H-001

Install Batteries in the 208 V UPS

NOTE: Each battery string consists of two battery modules and two short connectors.
  • The 10 kVA UPS contains two vertical battery strings installed in the left and right sides of the UPS.

  • The 15 kVA UPS contains two horizontal battery strings.

  • The 20 kVA UPS contains three horizontal battery strings.

  1. Remove the plate in front of the battery shelves.
  2. Holding the handle, install the batteries from the bottom and up in the indicated positions.

    10 kVA UPS

    15 kVA UPS

    20 kVA UPS

     
  3. Push down the handle of each battery module and fasten with the provided M5 screw in front of the battery module.
  4. Remove the shrink tubes from the power terminals and connect the power terminals to the batteries.
  5. Install the short connectors (from E3SOPT009) in the indicated positions.

    10 kVA UPS

    15 kVA and 20 kVA UPS

  6. Reinstall the plate in front of the battery shelves.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.