990-5940H-001

Overview of Single UPS

UIB Unit input breaker/switch
SSIB Static switch input breaker/switch
UOB Unit output breaker/switch
MBB Maintenance bypass breaker/switch
BB Battery breaker/switch
NOTE: Refer to Appendix: Switch/Breaker Details for the disconnecting device type.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.