990-6428B-001

Receiving

External Inspection

When the shipment arrives, inspect the shipping material for any signs of damage or mishandling. Check tilt and impact indicators. Do not attempt to install the system if a damage is apparent. If any damage is noted, contact Schneider Electric and file a damage claim with the shipping agency within 24 hours.

Compare the components of the shipment with the bill of lading. Report any missing items to the carrier and to Schneider Electric immediately.

Verify that labelled units match the order confirmation.

Remove the Modular Battery Cabinet from the Pallet

  1. Move the modular battery cabinet to the final installation area using a forklift.
  2. Remove the ramp from the top of the cabinet.
  3. Remove the shipping material.
  4. Remove the shipping brackets.
  5. Place the ramp and fasten it to the pallet with the provided bolts.
  6. Roll the modular battery cabinet down from the pallet.
  7. Move the modular battery cabinet to its installation location and use a wrench to lower the levelling feet. Ensure that the cabinet is level.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.