990-6428B-001

Install Batteries in the Modular Battery Cabinet

  1. Lockout/Tagout the BB battery breaker in the OFF (open) position.
  2. Remove the plate in front of the battery shelves.
  3. Cut the three cable ties that hold the battery cables to the frame.
  4. Remove the M6 screws from the battery shelves. Save the screws for future use.
  5. Holding the handle, install the battery modules one string at a time from the bottom and up.
    WARNING
    hazard of arc flash
    Be careful not to damage the battery cables when installing the battery modules. Lift the battery cables away from the battery shelves before pushing the battery modules into the cabinet.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  6. Push down the handle of each battery module and fasten with the provided screw in front of the battery module.

    Front View of Battery Module

  7. Remove the shrink tubes from the power terminals and connect the power terminals to the batteries.
  8. Reinstall the plate in front of the battery shelves.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.