990-6428B-001

Connect Power Cables

DANGER
hazard of electric shock, explosion, or arc flash
Do not drill or cut holes for cables or conduits with the gland plate installed and do not drill or cut holes in close proximity to the modular battery cabinet.
Failure to follow these instructions will result in death or serious injury.
NOTE: Route the signal cables separately from the power cables.
  1. Remove the conduit box from the rear side of the modular battery cabinet.

    Rear View of the Modular Battery Cabinet

  2. Rotate the conduit box and install.

    Rear View of the Modular Battery Cabinet

  3. Remove the gland plate from the top or bottom of the conduit box and drill holes for cables/conduits. Reinstall conduits (if applicable) and reinstall the gland plate.
  4. Remove the right side panel and the top cover.

    Front View of the Modular Battery Cabinet

  5. Route the power cables through the conduit box and connect to the busbars.
  6. If more than one modular battery cabinet is part of the installation, connect the battery cables between the modular battery cabinets.
  7. Reinstall the right side panel and the top cover.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.