DOCA0211EN-14

Audit Logs

The EcoStruxure Panel Server generates audit logs that record events such as invalid login attempts and firmware update.

The logs do not contain any personal information.

To detect unexpected behaviors (for example, frequent rebooting, incorrect firmware update, or invalid login attempts), it is recommended to monitor audit logs regularly. For more information about diagnostics logs, see DOCA0172•• EcoStruxure Panel Server - User Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.