DOCA0211EN-14

Firmware Update

Update the EcoStruxure Panel Server to the latest firmware version to obtain the latest features and keep up-to-date with security patches. All firmware designed for the EcoStruxure Panel Server is signed using the Schneider Electric Public Key Infrastructure (PKI) to help to provide integrity and authenticity of the firmware running on the EcoStruxure Panel Server. For proper PKI operation, keep the device date synchronized (see Date and Time).

To be informed about security updates, register with the Security Notifications on Schneider Electric Cybersecurity Support Portal.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.