DOCA0211EN-14

Recommended Actions for Cybersecurity

Your device is designed to be used in a protected environment that uses a defense-in-depth strategy.

To help secure your device, you must take specific actions at every stage of the project life-cycle.

NOTE: list of recommended actions below is not a complete list of possible cybersecurity measures. It is meant to be a starting point to improve the security of your device in a protected environment. Consult with cybersecurity experts to plan, configure, operate, maintain, and decommission your device based on your needs.

The following table lists the recommended actions for you to take to help secure your device in a protected environment, organized by life-cycle stage:

Life cycle stage Recommended action Defense-in-depth role

Plan

Review cybersecurity awareness.

Use available resources to increase your cybersecurity knowledge and awareness.

Review the system defense-in-depth assumptions. Follow the recommendations in this guide.

Understand the security measures expected to be provided by the external environment in which the device is to be used. These include, but are not limited to:

  • Site and device location security

  • Network security

Review the device security features. Refer to Security Capabilities in DOCA0172•• Panel Server User Guide.

Understand how the device security features can be used in a protected environment.

Review the security risks and compensation controls. Refer to Security Capabilities in DOCA0172•• Panel Server User Guide.

Understand known security risks and the compensation controls to help minimize the risks.

Install and configure

Check the state of the anti-tamper label before installation of the device.

Tamper-evident label prevents modification of the device before installation.

Follow the installation guidelines.

Help reduce unauthorized physical access.

Change the default password at first login. Refer to User Management in DOCA0172•• Panel Server User Guide.

Help reduce unauthorized access. Default account settings are often the source of unauthorized access by malicious users.

Change the Panel Server user password and Wi-Fi access point password. Refer to User Management and Wi-Fi Access Point in DOCA0172•• Panel Server User Guide.

Create strong passwords following the guidelines. Default account settings and weak passwords are often the source of unauthorized access by malicious users.

Disable unused protocols and ports.

Disable unnecessary and unused communication protocols and ports, for example, Wi-Fi, Wi-Fi access point, IEEE.802.15.4.

Operate

Encrypt backup configuration files.

Use strong passwords to encrypt configuration backup files. Unprotected files and weak passwords can be the source of unauthorized access by malicious users

Manage access to domains.

Limit access to known and required domains, according to your needs.

Report a cybersecurity incident or vulnerability.

Report suspicious activity, a cybersecurity incident, or a vulnerability to Schneider Electric Cybersecurity Support Portal web page.

Maintain

Maintain firmware up to date. Refer to Firmware Update in DOCA0172•• Panel Server User Guide.

Update to the latest firmware version to benefit from the latest security patches.

Monitor the audit log for unexpected behaviors. Refer to Diagnostics Logs in DOCA0172•• Panel Server User Guide.

Monitor the audit logs for unexpected activity and to help identify the cause of cybersecurity breaches that could lead to a cybersecurity incident.

Check the state of the anti-tamper label regularly.

Tamper-evident label prevents modification of the device.

Check the connected devices for the presence of unknown devices.

Locate and remove unknown devices to help protect the system against cybersecurity breaches.

Keep your network security up to date.

Helps reduce your attack surface, decreasing the likelihood of a vulnerability.

Perform security audits

Help verify the security status of your system.

Decommission

Reset the device to factory settings. Refer to Security Recommendations for Decommissioning in DOCA0172•• Panel Server User Guide.

Help prevent the potential disclosure of data.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.