DOCA0211EN-14

Modbus TCP/IP

A protocol which provides client/server communication between devices and TCP/IP that provides communications over an Ethernet connection.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.