DOCA0211EN-14

Device Disposal

The EcoStruxure Panel Server contains confidential information configured during commissioning, recent data values and logs. For example, this information can include Modbus device topology, wireless networks, Wi-Fi passwords, or measured power consumptions.

It is required to perform a factory reset before disposing of the EcoStruxure Panel Server. You must have physical access to power cycle the EcoStruxure Panel Server while executing this procedure. See how to reset EcoStruxure Panel Server to factory settings in DOCA0172•• EcoStruxure Panel Server - User Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.