DUG_Smart Radiator Thermostat_WH-00

Setting the room temperature manually

The room temperature can be increased/decreased manually by twisting the cap of the Thermostat.

Twist the Thermostat cap:

  • In the “+” direction to increase the temperature. The red LED will light up for 5 seconds.

  • In the “-” direction to lower the temperature. The blue LED will light up for 5 seconds.

When the Thermostat cap is twisted, the set-point temperature is increased/decreased by 2 °C from the current room temperature. The boost is active for 1 hour.

NOTE: If the set-point temperature is already more than 2 °C above or below the room temperature, a boost will not change the set-point temperature.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.