DUG_Smart Radiator Thermostat_WH-00

Setting the room temperature using the app

Using the Wiser Home app, you can adjust, set or boost the room temperature.

Precondition: Add a ELKO - Wiser Room Thermostat/ELKO - SmartSensor Climate Wireless in the same room where Thermostat is located.

To adjust, set or boost the room temperature:

  1. On the Control tab, tap All devices or a room tab where the Thermostat is located.

    1. Use the slider control on the right of the screen to adjust the temperature.

      NOTE: The flame shows that the room temperature is lower than the desired temperature (set point) and so the heating is ON.
      IMPORTANT:
      • When the boost time is set, the system automatically increases the set-point temperature by 2 °C for the duration of the boost. Once the boost period ends, the temperature returns to the last set-point.

      • Moving the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing.

      TIP: You can also adjust the room temperature:
      • By tapping or on the Control tab, in the Heating section of the concerned room to adjust its temperature.

      NOTE: If you only have a single device in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.
    2. Tap to set the boost time.

      IMPORTANT: Once the boost time is set, the set-point temperature automatically increases by 2 °C for the set boost time. After the boost time is over, the set-point temperature returns to the current scheduled event or to the previous set-point temperature.
      NOTE: Boost can be stopped at any time by tapping the and selecting it off.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.