DUG_Smart Radiator Thermostat_WH-00

Calibrating the device

The Thermostat calibrates the radiator valve, it adjusts the pin position, automatically after 5 minutes when batteries are inserted. It takes only a few seconds to do the calibration. You can hear the motor running sound when the Thermostat starts calibrating.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.