DUG_Smart Radiator Thermostat_WH-00

LED indications

Normal use

State

User Interaction

Left LED

Center LED

Right LED

Duration

Boost up

Twist the cap in the + direction

   

Solid for 5 seconds

Boost down

Twist the cap in the - direction

   

Solid for 5 seconds

Head calibration

State

User Interaction

Left LED

Center LED

Right LED

Duration

Start up

Insert the batteries

Single quick flash

Opening the valve

Automatic upon inserting batteries OR Twist and hold the cap in + direction for 8 seconds (for changing batteries)

   

Solid until the valve is open

Ready to install on the valve

The radiator thermostat is ready to install when the valve is fully open (see above)

 

Red and Blue: flash for up to 5 minutes

   

Orange solid = not joined

Green solid = joined

Closing the valve

Twist and hold the cap in the – direction for 2 seconds

   

Solid until the valve is closed

Joining

Twist and hold the cap in the + direction for 3 seconds

   

Pulses for up to 2 minutes

Joining success

     

Solid for 5 seconds

Joining failed

If no network is found after 2 minutes

   

Flashes for 5 seconds

Error state

State

User Interaction

Left LED

Center LED

Right LED

Duration

Low battery

     

Solid for 1 second (Repeated each hour)

Critical battery

     

Fast flash for 5 seconds (Repeated each minute)

No Signal

Twist the cap in the + direction to start a boost.

   

Fast flash for 5 seconds (Repeated)

No Signal

Twist the cap in the - direction to start a boost.

   

Fast flash for 5 seconds (Repeated)

No network

Twist the cap in the + or - direction to start a boost.

   

Solid with fade-out after 2 seconds. In this event, the radiator thermostat has not joined the wiser system and must either join the hub or be re-installed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.