DUG_SmartBlinds Puck_WH-00

About the device

The ELKO Smart Blinds Puck (hereinafter referred to as Puck ) provides the smart shutter functionalities with ordinary mechanical double push-button switches. The shutter Puck can be controlled directly from a wired-connected double push-button switch or wireless via the Wiser Home app.
Relay contacts are mechanically locked against each other to prevent simultaneous triggering of the two relay outputs.
NOTE: Do not use the Puck to control any devices depending on a permanent power supply.

Control options

Home control using Wiser app: To control the Puck through the Wiser Home app you will need the Wiser Hub. Refer to Pairing the device.

Direct operation: The Puck can always be controlled directly on-site. You can also connect it with mechanical double push-button switch. Refer to Manual operation.

Additional features:

  • Remote control with maximum of 10 mechanical double push-button switches.

  • Protection of the motor against damage, using two mutually mechanical and electronic locks between the relay contacts.

  • Protection against electronic overload, overheating and short-circuit.

  • Setting a schedule using Wiser Home app.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.