DUG_SmartBlinds Puck_WH-00

LED indication

Pairing the device

User Action

LED Indication

Status

Short press the Setup/Reset button or push button 3 times.

LED blinks orange once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for a few seconds before turning off.

Resetting the device

User Action

LED Indication

Status

Short press the Setup/Reset button or push button 3 times and hold it down once for > 10 s.

LED blinks red once per second.

The device is in reset mode. The device then restarts and LED turns orange indicating that the device is ready for pairing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.