DUG_SmartBlinds Puck_WH-00

Example of an automation

This demonstration shows how to create an automation that closes the Shutter when the Door is open during night time.
  1. Go to Automation > to create an automation.
  2. To add a condition, tap Add Condition > Device status change > Door Sensor, tap (A) to Open, then tap Set.
  3. Read the information and tap OK.
  4. To set the time, tap When > Add time > Period of time > Night time > Set.
  5. To add an action, tap Then > Add an action > Control a device > Micromodule Shutter > Set (B).
    TIP: You can set the required opening/closing percentage or fully open/closed state using the sliding bar.
  6. Read the information and tap OK.
  7. Enter the name of the automation.
    TIP: You can choose the cover image that represents your automation by tapping .
  8. Tap Save.
    Once the automation is saved, it is visible on the Automation tab.
    NOTE: You can enable or disable automations on the Automation tab by using (C).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.