DUG_SmartBlinds Puck_WH-00

Operating a Shades Control

You can operate the shades control using the Wireless switch.

Long press the top (ʌ) or bottom (v) of the Wiser Wireless switch (> 0,5 s) to move the shades control up or down.

  • Press to open the shades control (A)

  • Press to close the shades control (B)

  • Short press the top (ʌ) or bottom (v) of the Wireless switch (< 0,5 s) to stop the moving shades control (C).

  • Short press the top (ʌ) or bottom (v) of the Wireless switch (< 0,5 s) to adjust the slat position (D).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.