DUG_SmartBlinds Puck_WH-00

Resetting the device

You can reset the device to factory default manually.
Short press ( <0,5 s) the Setup/Reset button 3 times and then long press the Setup/Reset button once for 10 s to reset the Puck to factory default mode.
or
Short press the push button 3 times and then long press the push button once for 10 s.
After 10 s, the LED starts blinking red and then release the operation button.
NOTE: All configuration data, user data, and network data are deleted. After which
  • No connectivity to other devices or rooms

  • No timer settings

The LED stops blinking upon successful reset of the device.
The Puck restarts and blinks green for a few seconds.
NOTE: After reset, the LED turns orange indicating that the device is ready for pairing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.