DUG_SmartPlug 16A_ELKO_WH-00

Changing the icon and reassigning the equipment type

You can change the icon of the device.
  1. On the Home screen, tap > Devices > Smart Plug.
  2. Tap Icon, select an icon of the equipment type (A) and tap Save (B).
    IMPORTANT: If you have installed Plug and SmartTag, changing the icon to another category will delete all the historical data. Refer to Energy view of individual devices
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.