DUG_SmartPlug 16A_ELKO_WH-00

Using the device

The Device Control Screen allows you to switch ON/OFF the device and control various settings.

On the Control tab, select the plug and the control screen shows the options below.


A

Total energy consumption in the session

B

Tap to manually turn the device ON/OFF.

C

Tap to redirect you to the Schedule screen, where you can create a schedule. For more information, refer to the Creating a Schedule topic.

D

Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide

E

Tap to control various settings from the Device Settings screen. For more information, refer to the Configuring the device topic.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.