DUG_SmartPlug 16A_ELKO_WH-00

LED Indications

Pairing

User Action

LED Indication

Status

Press the operation button 3 times

LED blinks orange, once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning Off.

Resetting

User Action

LED Indication

Status

Press the operation button 3 times and hold it down once for > 10 s.

After 10 s, the LED starts blinking red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and the LED starts blinks green before turning Off.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.