DUG_SmartPlug 16A_ELKO_WH-00

Resetting the device

You can reset the device to factory default manually.
  1. Short press the operation button three times (< 0.5 s) and then long press the operation button once (>10 s).
  2. After 10 s, LED starts blinking red then release the operation button.
    The LED stops blinking upon successful reset of the device.
  3. The Plug restarts and blinks green for a few seconds.
    NOTE: After reset, the LED turns off.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.