DUG_SmartRelay Puck 10AX_WH-00

About the device

The SmartRelay Puck 10AX (hereinafter referred to as puck / micro module switch) combines the advantages of smart switch functionality with ordinary mechanical push-button switches. It transforms a conventional switch into a connected device that can be controlled from the switch or through the Wiser Home app. It can switch ohmic, inductive or capacitive loads.
NOTE: Do not control any devices that depend on a permanent power supply.

Control options

Home control: To control the puck through the Wiser Home app you will need the Wiser Hub.

Direct operation: The puck can always be controlled directly on-site. You can also connect any number of mechanical push-buttons.

Room control / Quick Home Connect: Operate the puck without a Wiser Hub.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.