DUG_SmartRelay Puck 10AX_WH-00

Pairing the device with the Wiser Hub

You can pair your puck with the Wiser Hub to access and control the puck.
  1. On the Home screen, tap .
  2. Tap Devices > > Lights > Micromodule Switch.
    TIP: You can also navigate by tapping Control > > Lights > Micromodule Switch.
  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the MAC Address and Install Code, then tap Connect. The app will verify if the MAC address and Install code are valid.

    • (B): Tap this option if you are unable to find the MAC address and Install code.

  4. Tap Next and select any one of the options to add the device:
    • Short press the Setup/Reset button 3 times on the puck with a screwdriver and make sure the LED blinks amber.
    • Short press the push button 3 times.
      NOTE: If the puck is located behind the push button, the status LED is not visible.

    Wait for a few seconds until the LED turns green and the app confirms that the device is joined.

    NOTE: If the LED is blinking green and red, see the instructions by tapping LED blinking green and red? or refer to the Troubleshooting topic.
  5. Tap Next to enter the name of the device and assign the device to a new room or an existing room. Then, tap Submit.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    The Puck is now listed on the Control tab under the All and Room tabs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.