DUG_SmartRelay Puck 10AX_WH-00

Manual operation

When the puck is connected to a mechanical push button, the connected devices can be controlled manually by short pressing the push button.

NOTE: When the puck is installed inside the wall box, the status LED is not visible while using the puck.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.