DUG_SmartRelay Puck 10AX_WH-00

Testing the device

Before using the puck, manually test it and make sure that it works when connected to the devices.

WARNING
HAZARD OF ELECTRIC SHOCK
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Short press the test button once, the connected device turns on/off.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?