ESXP2GE014EN-05

ASCO Medium and Low Voltage Architecture

In this architecture, data from the ASCO PTS (Power Transfer Switch), PCS (Power Control System), and from Load Banks and Generator Controllers are acquired by the ASCO CPMA (Critical Power Management Appliance) which can perform data processing and visualization. The processed data can also be displayed in the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation) for data visualization and reporting.

The recommended digital architecture to implement the Backup Power Testing application with the ASCO system is shown below:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?