ESXP2GE014EN-05

Medium Voltage Generator Architecture

The digital architecture of the Backup Power Testing application recommends direct Ethernet connections to the connected products. Data is captured on board connected products and uploaded into the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation) for data processing, visualization and reporting

The recommended digital architecture to implement the Backup Power Testing application with a medium voltage generator is shown below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.