Outputs
Outputs are displayed remotely via the Edge Control software EcoStruxure Power Monitoring Expert or Power Operation.
The Backup Power module of EcoStruxure Power Monitoring Expert must be deployed to benefit from the following features.
In the case of an ASCO architecture, outputs are displayed by the ASCO CPMA.
Live Data Display
The following outputs can be configured to represent an operator interface for Backup Power Testing:
Reports
The following reports can be generated on-demand or automatically generated and sent by email:
Backup/Emergency Power Reports
-
Generator Activity Report
Shows the test run hours and other test run data for each generator in the selected group.
-
Generator Load Summary Report
Provides a summary graph of electrical data during a generator run.
-
Generator Test (EPSS) Report
Provides a standard methodology for testing the generators and provides a detailed report of the generator operation during the test.
Can also be configured to conform to the requirements for a Backup/Emergency Power Supply System (EPSS)* test, including ATS/PTS*. For example, the report shows the transfer time of the lead ATS/PTS* and indicates whether the transfer time passes or does not pass the test requirements.

Backup Power System* Test Report
-
Generator Battery Health Report
Shows the captured waveform image of the generator voltage when the generator starts, compares it to a reference signature, and uses it to monitor battery performance over time and plan preventative maintenance actions when necessary.
Available with PowerLogic ION9000 only.
Uninterruptible Power Supply (UPS) Reports
-
UPS Auto-Test Report
Provides information regarding the battery health of your Galaxy VX/VL/VM/VS UPS devices.
-
UPS Battery Health Report (For third-party UPS)
Displays information related to the health of the battery for a UPS device. The UPS devices intended for use with this report are UPS devices that do not have an auto-test capability.
Available with PowerLogic ION9000 only.