ESXP2GE014EN-05

Inputs

Data from Generator

The following data are required:

Status, events, and diagnostic information:

  • Stopped, running

  • Generator starting, generator power availability (optional)

  • Power outage status (optional)

Electrical measurements:

  • Voltage (line to neutral / line to line)

  • Current

  • Total power, total apparent power

  • Power factor

  • Frequency

Engine analog measurements (optional):

  • Engine coolant temperature

  • Exhaust gas temperature

  • Engine oil pressure

  • Engine start battery voltage

This input data may be provided by the generator controller, the power control system (ASCO 7000 Series PCS), power meters (PowerLogic ION9000, PM8000, PM5000, ASCO 5210), data loggers (Cyber Sciences SER 3200/2408, ASCO 5112), and/or embedded metering (PowerLogic P5/P3, MasterPacT MTZ).

Data from Automatic Transfer Switch / Power Transfer Switch (ATS/PTS)

The following data are collected:

Status, events, and diagnostic information:

  • Normal, Test, Emergency

Electrical measurements:

  • ATS/PTS load data (optional)

This input data may be provided by the ATS/PTS controller (PowerLogic T300, ASCO 7000 Series PTS), power meters (PowerLogic ION9000, PM8000, PM5000), and/or data loggers (Cyber Sciences SER 3200/2408).

Data from Uninterruptible Power Supply (UPS)

The following data are collected:

Status, events, and diagnostic information:

  • Operating mode

  • UPS fault

  • Charger fault

  • Output overload

Electrical measurements:

  • Voltage and current (line to neutral / line to line)

  • Frequency

  • Battery voltage signature

These input data are provided by the UPS (Galaxy VX/VL/VM/VS).

Data from Load Bank (optional)

The following data are collected:

Electrical measurements:

  • Voltage (line to neutral / line to line)

  • Current

  • Total power, total apparent power

  • Power factor

  • Frequency

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?