ESXP2GE014EN-05

Low Voltage Generator Architecture

If the backup/emergency power system operates on a low voltage section of the network, it will usually include several ATS/PTSs*.

As illustrated below, the ATS/PTS* and the genset will each be equipped with a power meter that will collect analog electrical data from its power outputs as well as status details via digital I/O ports.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?