ESXP2GE012EN-05

Application Outcomes

Live Data Display

Capacity of electrical circuits can be visualized in an Electrical Health Diagram.

Events and Alarms

Smart alarms can be configured to alert energy managers or operations staff in case equipment capacity thresholds are exceeded.

Trends

Real-time and historical data can be viewed on a trend viewer.

Reports

  • Branch Circuit Power Report

  • UPS Power Report

  • Generator Capacity Report

  • Generator Power Report

  • Equipment Capacity Report

  • Power Losses Report

Notifications

SMS or email notifications are sent on pre-alarm and alarm conditions to enable fast action.

Cloud-Based Analytics and Services

As an option, EcoStruxure Service Plan powered by EcoStruxure Power Advisor can perform analytics based on historical data to provide insights and decision support. Issues related to electrical capacity of critical equipment, such as transformers, are shared with the user by our Schneider Electric service experts on a periodic basis with recommended actions to resolve them.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?