ESXP2GE012EN-05

Data Recording and Timestamping

For the Capacity Management application, a timestamp accuracy of ±1 second is sufficient for:

  • Time-based historical data visualization

  • Capturing peak power demand

  • Comparing peaks between different circuits for proper capacity planning

Advanced power meters such as the PowerLogic ION9000, PM8000, HDPM6000 and some PowerLogic PM5000 models (PM53xx and PM55xx) can timestamp and record onboard energy measurements. EcoStruxure Power Monitoring Expert or Power Operation can then retrieve the records with their original timestamp.

For other devices (PowerLogic P5/P3, MasterPacT MTZ, ComPacT NSX, Galaxy VX/VL/VM/VS, PowerLogic T300, ASCO 7000 Series PTS, entry level PowerLogic PM5000 models Acti9 iEM3000, PowerLogic PowerTag, etc.) measurements are acquired by the connected products and then recorded and timestamped by EcoStruxure Power Monitoring Expert or Power Operation.

NOTE: For devices without onboard logging, there is a possibility of data loss in the event of a communication failure.

For a comprehensive overview of device recording and timestamping capabilities, refer to Data Recording and Time Synchronization Capabilities of EcoStruxure Power Connected Products.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?