ESXP2GE012EN-05

Data Processing

Capacity Management data processing is embedded in the optional Capacity Management module of EcoStruxure Power Monitoring Expert or Power Operation.

Load Analysis

For branch circuits within a data center facility, average and maximum loading are tracked and compared to the circuit breaker size (A) to validate the design or to alert about potential overloading.

For an Automatic/Power Transfer Switch (ATS/PTS) or other equipment, peak load is compared with the rated capacity of the equipment to alert about potential overloading.

Power Capacity Analysis

For generators or UPSs, all related loads are compared with the remaining capacity to validate that a utility power outage could be handled while still complying with the intended redundancy design.

Power Loss Calculation

For transformers or UPSs, measurements performed at primary and secondary connections (in and out) are compared to establish power loss and associated cost.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?