ESXP2GE012EN-05

Inputs

The following data is required:

Electrical Measurements

The following electrical measurements are collected at strategic points of interest in the electrical distribution such as generators, Uninterruptible Power Supplies (UPSs), Automatic/Power Transfer Switches (ATSs/PTSs), feeders:

  • Current (A)

  • Active power (demand) (kW)

  • Apparent power (kVA)

  • Energy (kWh)

These data may be acquired from:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?