DOCA0150EN-09

About the Document

Document Scope

This document provides the firmware version history of FDM121 Ethernet display for one circuit breaker.

Validity Note

This document is valid only for FDM121 Ethernet display for one circuit breaker.

Online Information

The technical characteristics of the devices described in this guide also appear online. To access the information online, go to the Schneider Electric Country Website.

The information contained in this guide is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/ww/en/download/.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Product Related Cybersecurity Information

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
  • Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
  • Disable unused ports/services and default accounts to help minimize pathways for malicious attackers.
  • Place networked devices behind multiple layers of cyber defenses (such as firewalls, network segmentation, and network intrusion detection and protection).
  • Use cybersecurity best practices (for example, least privilege, separation of duties) to help prevent unauthorized exposure, loss, modification of data and logs, or interruption of services.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Environmental Data

For product compliance and environmental information, refer to the Schneider Electric Environmental Data Program.

Related Documents

The following table lists the documents that are compatible with a FDM121 display with the latest firmware version:

Title of documentation

Reference number

Enerlin'X FDM121 - Front Display Module for One Circuit Breaker - User Guide

ULP (Universal Logic Plug) System - User Guide

MicroLogic Trip Units and Control Units - Firmware History

DOCA0155EN

MasterPacT MTZ2/MTZ3 - IEC Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Unit From 800 to 6300 A - User Guide

To find documents online, visit the Schneider Electric download center (www.se.com/ww/en/download/).

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.