DOCA0150EN-09

Firmware Version 003.000.025

Bugs Fixed

The following bugs are fixed:

  • ComPacT NSX circuit breaker operation was not always possible after power restoration.

  • On the ground fault event, the current value Ig was not displayed as NA in Alarm History screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.