DOCA0150EN-09

Firmware Version 004.000.025

New Features

Supports MasterPacT MTZ circuit breaker with MicroLogic Active control unit and BCIM module to enable the following features:

  • Metering

  • Breaker status and control

  • Device identification

  • Reset (peak demand values, energy meters, minimum, and maximum values)

  • Maintenance (operation counters and load profile)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.