DOCA0150EN-09

Firmware Version 003.000.022

NOTE: The firmware version 003.000.022 is released through EcoStruxure Power Commission software.

New Features

Minor improvements in bar and dial graph screens.

Bugs Fixed

The following bugs are fixed:

  • Values were randomly not displayed in Quick View and Metering screens on change of Breaker System type or Breaker.

  • Product ID screen showed inconsistent pictures for ULP devices.

  • IO Lighting and Load control ON/OFF status was inconsistent with actual status.

  • Event pop-up was inconsistently displayed when user was in Quick View screen on power on.

  • Close Self Timer screen did not stop timer countdown on occurrence of an event.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.