DOCA0150EN-09

Firmware Version 003.000.013

New Features

The following features are added:

  • All 14 languages supported by default.

  • Improvement of the performance of the metering screen for reading values and navigation.

  • Added QR code display to access information about the FDM121 display.

  • Added new signature revocation mechanism to enhance cybersecurity.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.