DOCA0151EN-12

Firmware Version 6.4.2

New Features

  • Integrated the following devices:

    • Acti 9 Smartlink SI D gateway

    • Enerlin’X IFM Modbus-SL interface

  • For MicroLogic X control unit:

    • Integrated MTZ active alarms and alarm history

Bugs Fixed

  • In the General view grid, toggling of intermittent communication status resulted in unhealthy status, which is indicated in orange.

  • Auto-discovery did not always function when more than nine Modbus slave devices were connected to the same master gateway.

  • When IO modules were connected to a ComPacT NSX circuit breaker without a BSCM installed, the Quick view circuit breaker status was shown as Open.

  • For ComPacT NSX circuit breaker without a BSCM installed, some pages in Quick view display were shown as Not Responding in the title bar.

  • For MasterPacT MTZ circuit breaker, FDM128 displayed incorrect contact wear value in maintenance page.

  • For MasterPacT MTZ circuit breaker, FDM128 displayed incorrect power factor value in measures page.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.