DOCA0151EN-12

Firmware Version 8.0.19

New Features

  • Added Polish language

Bugs Fixed

  • Sometimes the FDM128 display stopped working when in the
    Measures (I) tab.

  • Low voltage circuit breakers were not discovered through Com'X or Link150 gateways.

  • Sometimes the MicroLogic Xi control unit connected through IFM interface (LV434000) was not discovered.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.