DOCA0151EN-12

Firmware Version 8.0.16

New Features

  • Integrated a new device – MicroLogic Xi

  • Added new events to monitor the internal Current Power Supply (CPS) sensors for MasterPacT MTZ circuit breaker.

Bugs Fixed

  • Temperature reading was not available after reconfiguring the analog input of IO module through EcoStruxure Power Commission software.

  • Volume in gallons was not supported for pulse counters configured on IO module.

  • Temperature in °F was not supported for PT100 sensor connected to an IO module.

  • Screen navigation, page numbering, and labels in the user interface had minor issues.

NOTE: The above bugs were observed in firmware versions 8.0.14 and 8.0.12.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.