DOCA0151EN-12

Overview

The FDM128 Ethernet display for eight devices (LV434128) is a 1-to-8 human machine interface (HMI). The main component is a 5.7-inch touchscreen.

An FDM128 display can be connected to devices via an Ethernet interface by using any of the following options:

  • One or more Ethernet gateways (IFE server, Link150, PowerLogic EGX300 and EGX100, PowerTag Link, PowerTag Link B, PowerTag Link HD, Smartlink SI B, or Smartlink Ethernet).

  • One or more third-party Ethernet gateways that possess the appropriate characteristics.

The FDM128 display monitors and controls up to eight devices from the following list:

  • Circuit breakers equipped with communicating MicroLogic trip units, such as:

    • MasterPacT MTZ circuit breakers

    • MasterPacT NT/NW circuit breakers

    • ComPacT NS circuit breakers

    • PowerPacT P- and R-frame circuit breakers

    • ComPacT NSX circuit breakers

    • PowerPacT H-, J-, and L-frame circuit breakers

    NOTE:
    • The information related to the new generation of ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers in this guide applies to the existing range ComPacT NSX and PowerPact H-, J-, and L-frame circuit breakers also. The exceptions are mentioned wherever applicable.

    • The information related to the new generation of ComPacT NS and PowerPacT P- and R-frame circuit breakers in this guide applies to the existing range ComPacT NS and PowerPact P- and R-frame circuit breakers also. The exceptions are mentioned wherever applicable.

    • These new ranges are based on the same technical and dimensional architecture as that of the existing range of circuit breakers.

  • Switch-disconnectors, such as:

    • MasterPacT NT HA switch-disconnectors

    • MasterPacT NW NA/HA/HA10/HF switch-disconnectors

    • ComPacT NS NA switch-disconnectors

    • ComPacT NSX NA switch-disconnectors

    • PowerPacT P- and R-frame switch-disconnectors

    • PowerPacT H-, J-, and L-frame switch-disconnectors

  • PowerTag Link devices, such as:

    • PowerTag Link gateway

    • PowerTag Link B gateway

    • PowerTag Link HD gateway

  • Smartlink devices, such as:

    • Smartlink SI B gateway

    • Smartlink Modbus gateway

  • EcoStruxure Panel Server devices, such as:

    • EcoStruxure Panel Server Universal

    • EcoStruxure Panel Server Advanced

    • EcoStruxure Panel Server Entry

The information displayed includes measures, alarms, and operating assistance data.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.