DOCA0151EN-12

Firmware Version 8.0.21

New Features

  • Integrated the following devices:

    • PowerTag F160 energy sensor (A9MEM1580)

    • PowerTag Rope energy sensors (A9MEM1590, A9MEM1591, A9MEM1592, and A9MEM1593)

    • ComPacT NSX and PowerPacT H-, J-, L-frame circuit breakers. These new ranges are the evolution of existing ComPact NSX and PowerPact H-, J-, and L-frame range of circuit breakers.

  • Added Instantaneous Protection status, Ii (On/Off) for MasterPacT NT/NW and MasterPacT MTZ circuit breakers.

Bugs Fixed

  • For MasterPacT MTZ circuit breaker:

    • The rate of Remaining Service life indicator was not updated correctly.

    • Energy per phase values were not displayed as per digital module availability.

    • In General view, the alarm status and circuit breaker status were not shown correctly when there was a high priority alarm.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.