DOCA0151EN-03

Firmware Version 6.4.2.2

Bugs Fixed

  • There was access competition to the same circuit breaker on the Modbus serial line between several masters.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?