Firmware Version 6.5.4
New Features
- 
                  
Integrated the following devices:
- 
                        
PowerTag energy sensors with part numbers A9MEM1560 to A9MEM1572
 - 
                        
Acti 9 OF24 indication auxiliaries
 - 
                        
Acti 9 SD24 indication auxiliaries
 - 
                        
PowerTag NSX energy sensors
 
 - 
                        
 - 
                  
For all MicroLogic trip units and control units:
- 
                        
Quick view additionally displays ampere protection settings: Ir, Isd, Ii, Ig, and IΔn.
 - 
                        
Safety message displays before opening and closing of the circuit breaker.
 
 - 
                        
 - 
                  
For MicroLogic X control units with firmware version 002.000.003 or greater:
- 
                        
Integration of additional events.
 - 
                        
Device view additionally displays:
- 
                              
Maintenance: load profile
 - 
                              
Measures: current demand and power demand
 
 - 
                              
 
 - 
                        
 - 
                  
For ComPact NSX circuit breakers with MicroLogic 7 trip unit:
- 
                        
Device view additionally displays earth leakage current.
 
 - 
                        
 - 
                  
For FDM128 display:
- 
                        
Selection of Modbus address range (between 1 and 247) before launching device discovery
 - 
                        
Pre-filling of gateway and device IP addresses according to FDM128 IP address and subnetwork mask
 - 
                        
Cancelation of device discovery in progress
 
 - 
                        
 - 
                  
Real time refresh rates Primary and Secondary renamed to Fast and Slow respectively.
 
Bugs Fixed
- 
                  
In General view, status of ComPact NSX and PowerPact H-, J-, L-frame devices was unstable.
 - 
                  
Bar graph was inconsistent with real-time current values for PowerTag devices.
 - 
                  
Text and graphics on display were misaligned.